LTE TDD
For Waveform Playback (ARB) capability.
The UL RMC Config button is displayed in the toolbar when the Uplink node is selected for a Basic TDD carrier.
Configures the uplink using the RMC (Reference Measurement Channel) configurations. One-shot action command (no query).
Comma-separated key:value argument; keys optional.
|
SCPI Command |
[:SOURce]:RADio:LTETdd:WAVeform[:ARB]:CCARrier<channel>:ULINk:CONFig:RMC "<string>" |
|
SCPI Example |
RADio:LTETdd:WAVeform:CCARrier1:ULINk:CONFig:RMC "SystemBandwidth:B5M,Modulation:QPSK,AllocatedRBs:25,RBPosition:LEND" |
|
Notes |
Comma-separated key:value (keys optional). Keys: SystemBandwidth (B1M4|B3M|B5M|B10M|B15M|B20M), Modulation (QPSK | QAM16), AllocatedRBs (1–100; valid set depends on bandwidth/modulation), RBPosition (LEND = lower end | UEND = upper end). |
|
Preset |
N/A |
|
State Saved |
No |
|
Initial S/W Revision |
A.20.01 |